Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to get the detail data between DTM in UP and X80 HART module
The communication bwteen DTM and HART module is HART over ethernet, we can capture the trace by wireshark at the service port of CRA if the HART is configured at the RIO Drop, the CRA service port should be configured mirroring the eth backplane.
Refer to the attachment picture, we can get the HART frame in the CIP data field, we can understand it following the HART command protocol.

Schneider Electric Nigeria

Attachment(s)
Microsoft PowerPoint - [Expert Support webinar - X80 HART Rev3- Jan. 28th.pptx]_2.jpg [90.27 KB]