Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Using XXMIT, XMIT, or L9_XMIT on Momentum, a loss of communications between a PLC Modbus Master and Slave is not detected
Issue
This Resolution is to inform users of Unity Momentum processors about an issue when using the XXMIT communication function block. The XXMIT, XMIT, and L9_XMIT will not exhibit an error 116 (communications timeout) in the 'Status' output word of the function block if the communications cable is removed between the master and slave device.


The XXMIT, XMIT, and L9_XMIT will not exhibit an error 116 (communications timeout) in the 'Status' output word of the function block if the communications cable is removed between the master and slave device.

The normal operating behavior of a broken media between a master and slave device is that an error 116 will be displayed in the STATUS output of the XXMIT function block.  In specific versions of Unity, an error 116 will not be observed.

The following table lists these conditions.
XXMIT with Unity VersionStatus Solution
8Fails – No error 116 displayed Upgrade to Unity 11
Install - HF1
Install - UnityPro_V110_HF0258202R
8.1Fails – No error 116 displayed Upgrade to Unity 11
Install - HF1
Install - UnityPro_V110_HF0258202R
10Functional– Error 116 is displayed No action required
11Fails – No error 116 displayed Install - HF1
Install - UnityPro_V110_HF0258202R


Product Line
171CBU78090

171CBU98090
171CBU98091



Resolution
Solution will be in Unity versions 11.1 and higher.


If Unity 11 is used, there are two additional HotFixes that must be installed to fix this issue.
  1. UnityPro_V110_HF0258202R (see attachment)
  2. UnityPro_V110_HF1 (can be found on www.schneider-electric.com or by launching SESU)

Schneider Electric Nigeria

Attachment(s)
UnityPro_V110_HF0258202R.7z [5.25 MB]