Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is an InF3 fault on an Altivar 12 drive?
Issue:
Altivar 12 with InF3 fault.

Product Line:
ATV12

Environment:
All serial numbers for ATV12

Cause:
N/A

Resolution:
This is an internal issue with the drive.
Power the drive down.
Once the display is blank, power the drive back up.
If the drive faults on InF3, a factory reset can be done by going to ConF menu and set FCS to InI (hold for 2 seconds).
Power cycle the drive.
If this does not fix the issue, it is recommended that the drive be replaced.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings