Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you clear the fault history in an ATV61 or ATV71 drive?
Issue:
Clearing the fault history in an ATV61 or ATV71 drive.

Product line:
ATV61, Altivar 61, ATV71. Altivar 71

Environment:
All

Cause:
Customer has a new installation, and it faulted on Main overvoltage.  They corrected the problem, and want to clear the history for the end user.

Resolution:
No, it is not possible to clear or reset the fault history on the drive.