Issue:
A customer wants to know the maximum onboard memory capacity for one of the EM4800 series meters.
Product Line:
EM4800 series
Environment:
EM4800 series product line
Resolution:
The onboard logs for the EM4800 series are capable of holding up to 2.4 years worth of data when configured at a 1 hour logging interval or 219 days at 15 minute intervals. The logging interval as well as the quantities to log can be configured through the EM4800 configuration utility.
A customer wants to know the maximum onboard memory capacity for one of the EM4800 series meters.
Product Line:
EM4800 series
Environment:
EM4800 series product line
Resolution:
The onboard logs for the EM4800 series are capable of holding up to 2.4 years worth of data when configured at a 1 hour logging interval or 219 days at 15 minute intervals. The logging interval as well as the quantities to log can be configured through the EM4800 configuration utility.
Released for: Schneider Electric Nigeria