Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Used Plastic Material Details in CT

1. Weights of plastic or other flammable materials (printed circuit boards)
Ans - The overall weight of plastic is 39.8 gram

2. Plastic details (Yellow Card- number according to UL 94) / the UL94 Flammability classification
Ans - Please find attached files for yellow card and datasheet of the plastic used in 16453 or METSECT5CC010

Schneider Electric Nigeria

Attachment(s)
LEXAN 500R Yellow Card.pdf [175.4 KB]
LEXAN 500R Data Sheet.pdf [26.42 KB]