Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the TSX Momentum modbus programming cable?
Issue
Part number for programming cable

Product Line
TSX Momentum

Resolution
The part number for the TSX Momentum modbus programming cable is a 110XCA20300 (DB9 - RJ45 Adapter) and one of the below 110XCA2820X  communication cable depending of length needed:

110XCA28201 RS232 Communication Cable—3ft, RJ45–RJ45.
110XCA28202 RS232 Communication Cable—10ft, RJ45–RJ45.
110XCA28203 RS232 Communication Cable—20ft, RJ45–RJ45.