Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to calculate the MC80 DIO channels
MC80 had modules HSC, DDM and Analogs fixed in its module. Sometimes user need the HSC but need more DI and DO, so we can propose user configure the HSC as DI and DO,
The questions is that how many channels of the HSC can be used
HSC DI channel 0, can be used as 6 x DI, and 2 x DO. make sure the 24V power supply for input and output connected.
HSC had two channels 0 and 1, so the DI is 12; DO is 4.The configuration page is at default.
Please refer to the attachments

Schneider Electric Nigeria

Attachment(s)
2.jpg [147.76 KB]
3.jpg [58.71 KB]
1.jpg [116.54 KB]