Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to upgrade a M580 V1 application in a M580 V2 application with Unity Pro V11
Due to compatibility issues, the “Change CPU” option was not allowed in Unity Pro V10 or V11 :  A M580 application with CPU V1.1 (developed with Unity Pro V8.0 or 8.1, or 10.0)  could not be updated to CPU V2.0
The hotfix UnityPro_V110_HF0300845R updates Unity Pro V11 installs a new tool to allow change M580 CPU from version 1.1 to 2.0.

This Hotfix is available on http://www.schneider-electric.com