Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you send an ASCII string out from a Schneider (Modicon) M340 or M580 with ModbusTCP/IP?

Product Line:
M340, M580, X80

Environment:
Ecostruxure Control Expert

Resolution:
Unfortunately, you cannot;
The M340 and M580 ethernet ports can only send or receive Modbus TCP/IP or Ethernet/IP messaging. They cannot read or write in ASCII characters using these protocols.
The only option is to use the M340 Modbus serial port or BMX NOM 0200 module with the INPUT_CHAR or the PRINT_CHAR function blocks to read and write an ASCII string to or from a server device.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings