Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
VA consumption for Link150
VA consumption for two different ports is as follows :
For 24 Vdc Mode : 24 Vdc,130 mA

For PoE Mode : 48 Vdc, 65 mA