Issue:
Specifications on the enclosed ATS22.
Product Line:
ATS22 Enclosed
Environment:
All serial numbers, enclosed ATS22
Cause:
Clarification of the specification of the ATS22
Resolution:
The specifications can be found in the Enclosed ATS22 Manual, document number 30072-453-26. The manual is attached below.
Specifications on the enclosed ATS22.
Product Line:
ATS22 Enclosed
Environment:
All serial numbers, enclosed ATS22
Cause:
Clarification of the specification of the ATS22
Resolution:
The specifications can be found in the Enclosed ATS22 Manual, document number 30072-453-26. The manual is attached below.
Released for: Schneider Electric Nigeria