Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Vijeo Designer v6.2 supports Windows 10?
Issue:
Is Vijeo Designer version 6.2 Windows 10 compatible?

Product Line:
HMI, Magelis, Vijeo Designer

Environment:
Windows 10

Cause:

Resolution:
Starting from Vijeo Designer 6.2 SP6, Windows 10 will be supported officially. All the documentation has been updated to reflect this in the Help menus and manuals.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings