Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a 110V I/O adapter available on Altivar Process drives?
Issue:
110V Input Output card for the Altivar Process drive

Product Line:
Altivar Process drives, ATV600, ATV900

Resolution:
We currently do not offer a 110VAC or 120VAC digital input adapter card for the Altivar Process series drives.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)