Issue:
VW3A1101 compatibility with the ATV600 and ATV900 Drives
Product Line:
ATV600 and ATV900 series
Environment:
All models, All serial numbers
Cause:
Information not available in current literature.
Resolution:
The VW3A1101 keypad is not compatible with the Altivar Process Drives. It is only compatible with ATV61, ATV71, ATV212, ATV312, and ATV32 Series Drives.
The keypad part number for ATV630 & ATV930 process drive is VW3A1111. An optional door mounting kit part number is VW3A1112.
VW3A1101 compatibility with the ATV600 and ATV900 Drives
Product Line:
ATV600 and ATV900 series
Environment:
All models, All serial numbers
Cause:
Information not available in current literature.
Resolution:
The VW3A1101 keypad is not compatible with the Altivar Process Drives. It is only compatible with ATV61, ATV71, ATV212, ATV312, and ATV32 Series Drives.
The keypad part number for ATV630 & ATV930 process drive is VW3A1111. An optional door mounting kit part number is VW3A1112.
Released for:Schneider Electric Nigeria