Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PME as an EWS server connected with SoapUI as an client got Error message 401.2

Issue:
When using PME as EWS server and SoapUI as an EWS client,SoapUI got the following error message:

<b> Error message 401.2 .: </b>Unauthorized: Logon failed due to server configuration. &nbsp;Verify that you have permission to view this directory or page based on the credentials you supplied and the authentication methods enabled on the Web server. &nbsp;Contact the Web server's administrator for additional assistance.<br><br>

Product Line:
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0

Cause:
This behavior is caused by Unauthorized, you have to put in the user name and password which has been authorized.

Resolution:
In SoapUI client, put in the username and password (e.g. username = supervisor; pw = 0​), every time before you use any Method or brose the items:
a