Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
If some desired value can be taken as the "base-level" of PIDFF
Question:
Customer would like the current valve position at the start of PIDFF block to be taken as the "base-level" output for the this block and it varies the output from there based upon setpoint and tuning parameters, is this possible?

Answer:
Customer could make use of the out_inf or out_min to achieve this base output value.

Schneider Electric Nigeria

Attachment(s)
pidsnap.png [18.85 KB]