Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV630 Process drive with Ethernet IP option card how do you set it up to use assemblies 103 and 104?
Issue:
ATV630  Process drive with Ethernet IP option card setting it up to use assemblies 103 and 104.

Product Line:
Altivar ATV630 ATV650 ATV660 etc

Environment:
All

Cause:
They needs to set up the ATV630 drive with the optional Ethernet IP card to use assemblies 103 and 104.

Resolution:
The ATV630 Ethernet IP card VW3A3720 does not support assemblies 103 and 104.  You will have to configure your PLC's Ethernet Scanner module for assemblies 100 and 101.