Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why my M241/251 controller stops in exception when an SD card is inserted?
One reason can be that the inserted SD card has no label.

To set the SD card label:
- open Windows file explorer
- select the SD card
- press F2 to rename it (for example : "mySDcard")