Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Trio Q & J Radio Multi-Use Serial Port Wiring

Overview

Both the Trio Q and Trio J radios have a multi-use serial port. Each radio features a 9 pin miniature D-Shell (DE-9) female connector that supports two individual serial port connections.

Typical use case for the J (unlicensed 900Mhz/2.4Ghz) or Q (licensed 150Mhz/450Mhz) radios will be Ethernet communications. Yet for legacy applications, a Modbus Gateway (Modbus TCP to RTU protocol converter), or Modbus Serial Device Server (Modbus RTU in TCP) may be configured on the serial port. A serial port may also be configured as a TUI (Text User Interface) for configuration/diagnostics. The TUI diagnostics is useful on systems suffering from high error rates as it provides a basic high speed interface.

Serial port configuration is accomplished with a web browser and the default IP address of both radios is 192.168.2.15. Details of how to configure each radio’s serial port for your application can be found in the Q or J radio documentation installed with TVew+.

Serial Port A & B (J series Radio)

Data Port A uses pins 2 & 3 with pin 5 as the common ground*
Data Port B uses pins 4 & 6 with pin 5 as the common ground*

Serial port pinout

RS-232 Mode
PinNameInput / Output
1Not Used---
2Port A RxDOutput
3Port A TxDInput
4Port B TxD (Diags)Input
5GND---
6Port B RxD (Diags)Output
7Not Used---
8Not Used---
9RSSI / General Purpose PinOutput



* There is no option for RS-485 connections with the J Series radio.

COM Port 1 & 2  (Q series Radio)

COM 1 uses pins 2,3,7 & 8 with pin 5 as the common ground
COM 2 uses pins 4 & 6 with pin 5 as the common ground

serial port DB9

RS-232 ModeRS-485 Mode
PinNameInput / OutputNameInput / Output
1COM 1 DCDOutputNot Used---
2COM 1 RxDOutputB / Z (Inverting)Input / Output
3COM 1 TxDInputA / Y (Non-Inverting)Input / Output
4COM 2 TxDInputNot Used---
5GND---Not Used---
6COM 2 RxDOutputNot Used---
7COM 1 RTSInputNot Used---
8COM 1 CTSOutputNot Used---
9RSSIOutputRSSIOutput