Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the motor current be permanently displayed on the display of an ATS22 Softstart?
Issue:
Motor current permanently on the display of the ATS22

Product Line:
Altistart 22

Environment:
All Serial number

Cause:
Product feature

Resolution:
Currently, there is no way to select the current to be permanently displayed for the status.
This is possible in our drives and the ATS48, but not in ATS22.