Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum number of drives you can daisy chain using Modbus TCP/IP on an ATV32
Issue:
Maximum number of drives to daisy chain

Product Line:
ATV32, ATV61 and ATV71

Environment:
Modbus TCP/IP
Daisy chain part number
ATV32 - VW3A3616
ATV71 or ATV61 - VW3A3310D

Cause:
None

Resolution:
The maximum number of devices is 32.  However, there may be some limitations.  Please see the attached.

Schneider Electric Nigeria

Attachment(s)
ATV in Ring or daisy chain topology.pdf [76.25 KB]