Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the StUn parameter for the ATV32 Drive?
Issue:
Customer was asked to change StUn to CUS per the machine OEM, but he is unable to change this value

Product line:
Altivar 32, ATV32

Environment:
all

Cause:
n/a

Resolution:
The StUn parameter for Tune Selection is a Read only parameter, found in the drC menu.

The factory setting is tAb (Default).
If an autotune is completed, this value changes to MEAS (Measured).
To change this value to CUS (Custom) the motor measurements must be manually entered and saved.