Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to copy alarm messages between Vijeo Designer applications?
Issue:
How to copy alarm messages between Vijeo Designer applications?

Product Line:
Vijeo Designer

Resolution:
The alarm messages are embedded in the variables.  To copy the alarm messages between two identical project, export the variables from one project and import it into the other project.  Assuming that the variables name are the same.