Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PM8000, ION7400, and ION9000 I/O option modules installation guide
Issue
User is trying to locate and download the installation guide for PM8000/ION7400/ION9000 I/O option modules.

Product Line
METSEPM89M2600
METSEPM89M0024

Environment
PM8000 series meters
ION7400 series meters
ION9000 Series meters

Resolution
METSEPM89M2600 is part# for the I/O option module for PM8000, ION7400, and ION9000 series meters that have 2 relay outputs and 6 digital inputs
METSEPM89M0024 is parti# for the I/O option module for PM8000, ION7400, and ION9000series meters that have 2 analog outputs and 4 analog inputs.

See the installation guide for METSEPM89M2600 from here.
See the installation guide for METSEPM89M0024 from here.