Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How low can the motor thermal current be set on the ATV12 drives when you are running a smaller size motor on the drive?
Issue:
Set motor thermal current on the ATV12 drives when you are running a smaller size motor.

Product Line:
Altivar 12

Environment:
All

Cause:
Wants to know what is the smallest size motor you can put on the ATV12 drive and still have motor thermal protection.

Resolution:
You can program the Nominal drives motor current to 25% of the drives current IN ratings.