Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to disable CM4000T Flicker alarms
Issue
The user is unable to disable CM4000T’s Flicker alarms in ION Setup. As shown below, the flicker alarms found in the standard alarm setup are not enabled.
Standard Alarm Setup

Product Line
CM4000T

Environment
ION Setup

Cause
The Power Quality Summary Configuration forces Flicker alarms to stay enabled

Resolution
Navigate to the Power Quality folder after selecting your CM4000T in ION Setup.
The Power Quality Summary Configuration option needs to be disabled in the CM4000T to restrict Flicker alarms.
Power Quality Summary Configuration

After it is disabled, Flicker alarms will be disabled.
PQ Summary

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: