Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What level of leakage current the ATV61/71 will detect a Ground Short Circuit Fault?
Issue:
Looking for the level of leakage current the ATV61/71 that detects a Ground Short Circuit Fault

Product Line:
All ATV61/71 drives

Environment:
Ground Fault detection

Cause:
N/A

Resolution:
The level of leakage current the ATV61/71 which detect a Ground Short Circuit Fault is above 25% in the ATV61/71 Drives.