Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the replacement filter boards for the ATS48 soft starters?
Issue:
Needs the replacement filter boards for the ATS48 soft starters.

Product Line:
Altistart 48  ATS48

Environment:
ATS48D17Y – ATS48C32Y

Cause:
Replacement

Resolution:
The replacement filter board is selected based on the ATS48 part number.
There is one filter board per ATS48.
See the attached file.

Schneider Electric Nigeria

Attachment(s)
ATS48 filter boards.pdf [186.62 KB]