Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
what’s the material declaration for Premium PLC parts
Question:
What’s the material declaration for Premium PLC parts?

Answer:
As for premium offers, we only have the first 6 items of Table(listed below) since they are RoHS substances.
Be noticed that =S= complies with RoHS Regulation of European so that the threshold value was not exceeded except for some RoHS exemptions.
The exemptions are applied in specific circumstances which is to be referred at further inquiry based on applied case.

Schneider Electric Nigeria

Attachment(s)
material.png [5.87 KB]