Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the resolution of the BMXART0814 .
The BMXART0814 has a resolution of .1 degrees. ( Read as 1/10 degree Fahrenheit or Celsius.)
The BMXART0414 has the identical resolution.