Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
My SoMachine controller stops in exception for no obvious reason and I have some function blocks declared as retain
In Somachine v4.x it is not possible to declare function blocks as retain as this can cause exceptions.
But it is still possible to declare variables as retain inside function blocks.

Declaring function blocks as retain is possible with Machine Expert.
(Note that retain variables consume less memory than full function blocks).