Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a fix for the M580 10 year offset issue with the BMXNOR0200H?

Issue
M580 10 year offset issue with the BMXNOR0200H

Product Line
M580 CPU modules

Environment
Unity Pro, Control Expert


Resolution
From the release notes for the M580 CPU firmware version 2.12 - The Fix for the 10 years offset issue when the time reference for NTP is coming from BMXNOR0200 is added to firmware version 2.12 or higher.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)