Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a port number other than Modbus/TCP port 502 be used for I/O Scanning on the 140CPU6x..x native ethernet port?

Product Line:
Quantum PLC

Environment:
EcoStruxure Control Expert

Resolution:
No,
the Quantum 140CPU6x..x Copro native ethernet port will only use Modbus TCP port 502 when performing an I/O Scanning function.
Port 502 is hard-coded into the Ethenet port settings and is not configurable.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)