Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What do the LED status indications mean on the HMI screen of the Altivar 630 and 930 process drives?
Issue:
Where can I get a documentation that explains the LED status indications on the HMI screen of the Altivar 630 and 930 process drives?

Product Line:
Altivar 630/930

Environment:
All serial numbers for Altivar 630/930

Cause:
N/A

Resolution:
LED indicators

Schneider Electric Nigeria

Attachment(s)
Altivar_Process_HMI.pdf [48.68 KB]