Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which systems can I configure using Config ELEC?
Config ELEC handles the configuration of the following systems :
• Wiserlink with a MIP.
• Acti9 Smartlink ELEC
Wiserlink without MIP, WiserSmart, Acti9 Smartlink SI (between others) are not supported.