Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Please advice if there is recommendation for the earthing of the LTMR (Motor protection relay).
If the product case is plastic , therefore the product does not need a external earth connection for the same potential and that's why TeSys T does not have earth connection terminal.

Also the second reason for that is TeSys T has doubled isolation and hence do not require earthing.