Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which PDUs are used in the SmartBunker SX and CX?
Issue:
A customer is asking which PDU is included in the SmartBunker SX and CX.

Product Line:
SmartBunker SX and CX

Environment:
All versions and serial ranges.

Cause:
Customers want to know which PDU comes with the SmartBunker SX or CX.

Resolution:
PFMSB30024NA ships with AP7902.
PFMSB30042NA ships with AP8958NA3.
PFMSB40024NA ships with AP7902 and AP9567.
PFSMB40038NA ships with AP8958NA3.