Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a library of graphical objects in Vijeo Designer?
Issue:
Looking for a way to draw some professional looking images on the HMI screen. Where can I find some sample images to use in my Vijeo Designer application?

Product Line:
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer's toolchest, there are two folders with many different graphical objects that are used by the various industries. The names of these folders are:

Image Library
Schneider Electric Image Library

Please have a look in these folders to see if there is something that fits your requirement.

If you do not find what you need, you can also import a PNG, BMP, JPG, or EMF file in Vijeo Designer using the image object.