Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to configure the Unity Pro LL984 network display view
Follow this procedure for configuring the Unity Pro LL984 network logic screen. In this example we will configure the screen to show two descriptor lines, the variable and the 984-address.



1- Go to the TOOLS tab and select PROJECT SETTINGS.
2- In the Project Settings window, select View 1 from the Network Display option.
3- Configure the following:
Line 1 = Blank
Line 2 = Blank
Line 3 = Blank
Line 4 = Descriptor 1
Line 5 = Descriptor 2
Line 6 = Variable
Line 7 = 984-Address
4- Click the APPLY button, then the OK button.
5- The LL984 Network Display View will now show the descriptors, variable and 984-address.