Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the replacement temperature sensors for the ATS48 soft starters?
Issue:
Part number of temperature sensors for the ATS48 soft starters?

Product Line:
Altistart 48  ATS48

Environment:
All models

Cause:
Replacement

Resolution:
The replacement temperature sensor is selected based on the ATS48 part number.
There is one sensor per ATS48.
See the attached file.

Schneider Electric Nigeria

Attachment(s)
ATS48 Temp Sensor.pdf [187.97 KB]