Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are fast screws sufficient to ensure the holding of the frame of my Resi9 Electrical Panel on Insulatin backpart?
Yes, the screws supplied with the chassis are sufficient (installed according to the description in the manual) if you are using the Plus backpart