Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Terminate All Sessions Prior to Restoring a Database

Issue
Cannot restore a database.  The Restore Database operation fails, reporting that exclusive access could not be obtained because the database is in use.

Product

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024



Environment
SQL Server

Cause
Before an existing database can be restored, there should be no connections using the database. If the database is currently in use the RESTORE command fails with below error:

Msg 3101, Level 16, State 1, Line 2
Exclusive access could not be obtained because the database is in use.
Msg 3013, Level 16, State 1, Line 2
RESTORE DATABASE is terminating abnormally.

Resolution
To avoid this, we need to terminate all sessions that use the database. All sessions using the database can be obtained
by executing the system stored procedure sp_who2 or by querying the sys.dm_exec_sessions table as:
SELECT   session_id
FROM     sys.dm_exec_sessions
WHERE    DB_NAME(database_id) = 'RestoringDatabaseName'

You need to terminate each of the sessions returned individually by using KILL command.

If there are a large number of sessions to terminate, or you need to do this on a routinely,this can be a lengthy and tedious process.
You can *automate* this using below script, which takes the database name as input, and terminates all sessions connecting to it.

USE [master]
GO
 
DECLARE @dbName SYSNAME
DECLARE @sqlCmd VARCHAR(MAX)
 
SET @sqlCmd = ''
SET @dbName = 'RestoringDatabaseName' -- Change database name here
 
SELECT   @sqlCmd = @sqlCmd + 'KILL ' + CAST(session_id AS VARCHAR) +
         CHAR(13)
FROM     sys.dm_exec_sessions
WHERE    DB_NAME(database_id) = @dbName
 
PRINT @sqlCmd
 
--Uncomment below line to kill
--EXEC (@sqlCmd)
As in example the script and results will look like this
Script

** see attachment containing the SQL script text

Schneider Electric Nigeria

Attachment(s)
TerminateSessions.txt [382 Bytes]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: