How can we help you today?

Does BMXNOM0200 module support protocol of ANSI Specification X3.28-1976, Subcategory E3

Question:
Does BMXNOM0200 module support protocol of ANSI Specification X3.28-1976, Subcategory E3?

Answer:
No, we do not support this protocol as a standard. On the other hand, it could be managed by the PLC application using the BMXNOM0200.