Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which is the correct variable for MV presence which co-relates to pin no. 8 of Mate N-Lok 9 pin connector in T200S ?

1.1 - Question

Which is the correct variable for MV presence which co-relates to pin no. 8 of Mate N-Lok 9 pin connector in T200S ?

1.2 - Application

This FAQ is applicable when it is required to identify correct variable for a digital input for MV presence.

1.3 - Answer

The variable Aux._MV_Presence_x (TSS54 for switch-1 and TSS85 for switch-2) co-relates to pin no. 8 of Mate N-Lok 9 pin connector in T200S. These two are the only variable for voltage presence/absence, which will be used by Automatism function for switch-1 (TSS54) and switch-2(TSS85) in T200S.


The variable MV_Presence_x (TSS73 and TSS105) are for T200P, where it will be derived from Voltage measurements.

1.4 - Performance

The automatism function will work perfectly fine when Aux._MV_Presence. This digital input is used to detect voltage presence or absence for respective switch.

Schneider Electric Nigeria

Attachment(s)
FAQ_T200S_MV_Presence.pdf [117.94 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings