Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What analog inputs are available on the ATV630 Process Drive?

Article available in these languages: Spanish

Issue:
ATV630 process drive analog inputs available.

Product line:
Altivar Process, ATV630, ATV600, Altivar 630

Environment:
All serial numbers

Cause:
n/a

Resolution:
The ATV630 drive comes with three analog inputs.  Each is programmable to be used for voltage or current.

The Min and Max Values are independently adjustable to allow setting up as voltage or current speed reference for most applications.  For example, 0-10V, 2-10V, 4-20mA, 20-0mA, etc.

Schneider Electric Nigeria

Attachment(s)
ATV600 analog inputs.jpg [36.7 KB]