Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How do I program my ATV312 drive to run in reverse via logic input?
Issue:
Program my ATV312 drive to run in reverse via logic input

Product Line:
ATV312 series drives.

Environment:
All models, All serial numbers.

Cause:
Unable to find directions in existing literature.

Resolution:
The rrS parameter, under the I-O menu is used to assign "run reverse" to a logic input.  By default, this is assigned to LI2 if the drive is in 2 wire control, and LI3 if the drive is in 3 wire control.