Search FAQs
Is a time delay available on the ATV312 logic inputs?
Issue:
Time delay feature on the ATV312 logic inputs
Product line:
Altivar 312, ATV312
Environment:
all
Cause:
Delay before activation
Resolution:
The Altivar 312 does not offer a delay time for the Logic inputs. An external timer can be added if needed.
Time delay feature on the ATV312 logic inputs
Product line:
Altivar 312, ATV312
Environment:
all
Cause:
Delay before activation
Resolution:
The Altivar 312 does not offer a delay time for the Logic inputs. An external timer can be added if needed.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: