Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which base units are compatible with XVUZ12 installation in XVU range?
The compatibility of XVUZ12 in XVU range as below:
XVUZ02, XVUZ02Q, XVUZ03, XVUZ400, XVUZ800, XVUZ05.