Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Getting error E7701 on LXM32 drive
Issue:
Getting E7701 on the LXM32 drive

Product Line:
LXM32

Resolution:
E7701 is a system error: Timeout during connection to power stage.
The drive will have to be replaced. This error cannot be reset.